SLVSMQ4 September 2026 TPS7H5101-SEP
ADVANCE INFORMATION
Packet Error Checking (PEC) can optionally be utilized to provide error checking on data transmissions. If the TPS7H5101 receiver receives data from the controller that does not match the calculated PEC, the TPS7H5101 performs a NACK the of the PEC byte. Additionally, the command is not acted upon and the CML bit is set in the STATUS_BYTE register.
If the controller provided clock pulses are provided before a STOP, PEC is used. If the STOP is issued without extra clock pulses, PEC is not used. Though the PEC is optional, utilization of this feature is recommended for robust and reliable data transmissions.