SLVUCP9B November 2023 – October 2025
To generate a new customization configuration for the TPS25751 device, click the Reset Configuration button on the top right side of the tool (this is next to the Flash To Device drop-down menu). This button erases the existing configuration and resetting the form back to the default settings. TI recommends to export the existing form first so that the existing configuration is not lost. Refer to Section 3.3.6.2 for details on how to save configurations.