Enable the TLV61290EVM board for operation by the following steps:
- Set J10 to the ON position. Turn on the power supply.
- Open the GUI.
- Click the Auto Connect button one bottom left corner of the page on the target address widget (Figure 3-2). This automatically checks for target addresses (0x75, 0x76, 0x77) and connect the GUI with the device.
- Click the Start button. This shows the GUI user interface of TLV61290EVM-076 (Figure 3-3).