SLVUDH9 March   2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Hardware Description
    2. 2.2 Power Requirements
      1. 2.2.1 Power Tree
        1. 2.2.1.1 On-Board Power Supplies
        2. 2.2.1.2 Analog Voltage Reference
        3. 2.2.1.3 Alternative Power Sources
          1. 2.2.1.3.1 USB Isolation
          2. 2.2.1.3.2 External Power Connections
          3. 2.2.1.3.3 5V Step-Up Converter
      2. 2.2.2 Power Indicator LEDs
    3. 2.3 Reset
    4. 2.4 Clock
    5. 2.5 Interfaces
      1. 2.5.1 User LEDs
      2. 2.5.2 MCAN
      3. 2.5.3 Encoder Connectors
    6. 2.6 Debug Interface
      1. 2.6.1 XDS110 Debug Probe
      2. 2.6.2 Virtual COM Port
      3. 2.6.3 ARM 10-Pin Debug Header
    7. 2.7 Test Points
    8. 2.8 BoosterPacks
  9. 3Additional Information
    1. 3.1 Revision E1 Appendix
      1. 3.1.1 Revision E1 Known Issues
    2. 3.2 Revision E2 Appendix
      1. 3.2.1 Revision E2 Changes from E1
    3. 3.3 Trademarks

Reset

nRST

The AM13E230x MCU reset is controlled by the nRST pushbutton S1. The nRST net is also connected to BoosterPack header J2-16 so the MCU reset can be controlled by an external circuit if desired. The nRST input to the AM13E230x MCU is an active low signal.

BSL Invoke

An additional reset pin can also be user-controlled on the LaunchPad. The BSL (Boot Strap Loader) Invoke signal triggers a system reset and allows the Boot Configuration Routine (BCR) to run the Bootstrap Loader. The BSL Invoke pin assignment is user configurable, and has been assigned to pin PA6 (GPIO6). BSL Invoke is configured as active high on the LaunchPad.

By default, the BSL Invoke signal is generated by the XDS110 firmware as part of the boot routine and is output from the XDS110 (U15) pin PF0. To disconnect this signal from the XDS110 and use the on-board pushbutton S5 to generate the BSL Invoke signal, the following jumpers must be removed and installed:

  1. Remove the jumper on J12 connecting the BSL Invoke net from the XDS110 to the AM13E230x MCU (denoted by BSL INV on the PCB silkscreen).
  2. Populate a jumper on J11 to connect the output of the pushbutton S5 to the AM13E230x MCU
LP-AM13E230 Changing BSL INV to Pushbutton Figure 2-5 Changing BSL INV to Pushbutton

GPIO Wake

A dedicated GPIO used to wake the AM13E230x MCU from low power modes is connected to push button S2. This push button can also be used for a user GPIO input to the AM13E230x MCU. GPIO45 (PB13) is assigned as the WAKE GPIO as it can wake up the MCU from SHUTDOWN mode, the lowest power consumption mode on the device. MCU WAKE is configured as an active low signal on the LaunchPad.