SLVUDH9 March 2026
Two user-controllable LEDs are provided on the EVM: LED4 (RED) and LED5 (GREEN). The LEDs are driven by an LED Driver IC SN74LVC2G07 (U10). LED4 is connected to pin PA5, and LED5 is connected to pin PB0. The LEDs are connected in an active-low configuration; when the MCU GPIO is driven low, the LED turns on, and when the GPIO is driven high, the LED turns off. These LEDs are dedicated for use by software applications.
| LED Designator | Description |
|---|---|
| LED4 | Active-low user-configurable RED LED controlled by PA5 |
| LED5 | Active-low user-configurable GREEN LED controlled by PB0 |
Figure 2-7 LP-AM13E230 User LEDs