SLVUDH9 March 2026
The AM13E230x MCU default clock source on the LaunchPad is a 25MHz crystal oscillator (Y1) connected to the X1 and X2 pins of the MCU, and is referred to as XTAL. Alternatively, a high frequency digital clock input ranging from 4-48MHz can be connected to J14, and is referred to as HFCLK_IN.
In order for HFCLK_IN to be the main external oscillator input, there are a few hardware modifications required to the LaunchPad:
The AM13E230x MCU CLKOUT pin is accessible on header J15. The external clock output is useful for clocking external circuitry such as an external ADC that does not have a clock source. The clock output unit on the AM13E230x MCU has several sources and a programmable clock divider. For information on configuring the CLKOUT unit, refer to the Technical Reference Manual.