SLVUDM1 November 2025
Click on the IO Configuration icon in the left side column of the window and the following window is displayed.
The IO configuration window is setup with the default settings. Both SPDIF inputs and the USB inputs need the I2S inputs.
If an external I2S or TDM signal is provided the inputs and outputs are configured in this window.
The Serial Port configuration is set when PPC3 connects to the EVM.