SLYU067 December   2023 DRV5011 , DRV5012 , DRV5013 , DRV5013-Q1 , DRV5015 , DRV5015-Q1 , DRV5021 , DRV5021-Q1 , DRV5023 , DRV5023-Q1 , DRV5032 , DRV5033 , DRV5033-Q1 , DRV5053 , DRV5053-Q1 , DRV5055 , DRV5055-Q1 , DRV5056 , DRV5056-Q1 , DRV5057 , DRV5057-Q1 , TMAG3001 , TMAG5110 , TMAG5110-Q1 , TMAG5111 , TMAG5111-Q1 , TMAG5115 , TMAG5123 , TMAG5123-Q1 , TMAG5124 , TMAG5124-Q1 , TMAG5131-Q1 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5231 , TMAG5253 , TMAG5273 , TMAG6180-Q1 , TMAG6181-Q1 , TMCS1107 , TMCS1108

 

  1.   1
  2.   Trademarks
  3.   Abstract
  4. 1Introduction and Features Overview
    1. 1.1 Simulating Magnetic Fields Tool Introduction
  5. 2Simulation Interface
    1. 2.1 Getting Started
    2. 2.2 Creating a New Design
    3. 2.3 Selecting a Sensor
    4. 2.4 Sensor Output Types
  6. 3Simulation Environment
  7. 4Simulation Inputs
    1. 4.1 Magnet Input Fields
      1. 4.1.1 Magnet Specifications
      2. 4.1.2 Magnet Geometry
      3. 4.1.3 Magnet Motion
      4. 4.1.4 Magnet Rotation
      5. 4.1.5 Hinge Magnet Motion
      6. 4.1.6 Linear Magnet Motion
      7. 4.1.7 Joystick Magnet Motion
    2. 4.2 Sensor Input Fields
      1. 4.2.1 Linear Sensor Format
      2. 4.2.2 Latch and Switch Format
      3. 4.2.3 Sensor Position
    3. 4.3 Simulation Settings
  8. 5Simulation Results
  9. 6Parametric Sweeps
  10. 7Comparing Designs
  11. 8Summary
  12. 9References
  13.   A Appendix
    1.     A.1 Sensor Placement
    2.     A.2 Magnet Materials
    3.     A.3 Rotation Tips

Sensor Input Fields

The specific sensor selected and the location of that sensor in the simulation directly influences the output behavior observed. The goal of TIMSS is to help evaluate what this output is. Placing the sensor anywhere to compare similar devices at the same location helps in selecting the correct sensor for any design, including overlapping with other sensors. Up to six sensors can be placed in any simulation (Figure 4-10).

GUID-20231114-SS0I-LMP2-CC1F-L2FK7TV4WXVW-low.svg Figure 4-10 Sensor Selection Menu

Select sensors for use in the simulation at any time by clicking Edit Sensor Selection. All user inputs tied to the sensor are deleted once a sensor is removed.

Using different settings for each sensor is possible. Select the drop-down arrow to expand the list of sensors and switch between sensor settings (Figure 4-10).

Each device is set to a specific oderable part number and the fields of the form automatically update with all the relevant specifications that govern device response. There are generally two formats: one for linear devices and another for latches and switches.