SNAA408 April 2025 LMK3H0102
Running a trace through a via causes a disruption in the current flow, which is likely to cause an EMI spike. However, having vias significantly larger than the trace width creates an even harsher transition (Figure 1-1). This harsher transition can act as an antenna, creating larger EMI spurs. When running a trace through a via, have the trace width be slightly larger than the via (Figure 3-7).
Figure 3-6 Passive with Narrow Trace