SNAA408 April 2025 LMK3H0102
A large passive component pad connecting to a smaller trace width can also be a source of EMI spikes (Figure 3-8). When connecting the passives, have the trace width match the pad size. Similarly, when connecting a net between two planes, use several vias to distribute the energy more evenly (Figure 3-9). This is especially crucial for power and ground nets.