SNAA408 April 2025 LMK3H0102
Spread Spectrum Clocking (SSC) is the most commonly used tactic to mitigate this source of EMI. SSC is able to reduce the peak amplitude of a digital clock signal by shifting the frequency in a controlled manner, thereby distributing the energy in the frequency domain. This does not, however, affect the amplitude of the clock in the time domain. Center-Spread SSC spreads the energy evenly on either side of the target frequency. Down-Spread SSC only spreads the energy to frequencies below the target. Both versions of SSC can vary in intensity. Figure 2-3 shows the results for 0% (blue), ±0.5% (green), ±1%(cyan) and ±2% (red) center-spread SSC. Clocking devices such as the CDCE6214 and the LMK3H family have SSC capability.

More information can be found in the Spread Spectrum Clocking Using the CDCS502/503, application note.