Design of all aspects of the LMK3H0102-Q1 is straightforward, and software support is available to
assist in frequency planning and part programming. This design procedure gives a
straightforward outline of the process.
- Frequency Planning
- The first step of designing an LMK3H0102-Q1 configuration is to determine the FOD
frequencies that are required to generate the required output
frequencies. The process is as such:
- If the output
frequencies are greater than 200MHz, the frequencies must both
be the same, and can not use SSC. If the frequencies are
different, or require SSC, then this frequency plan can not be
supported by the device.
- In the
case of two identical frequencies greater than 200MHz,
the edge combiner must be enabled, the FOD divider
values must match, and REF_CLK, if used, can be sourced
from either FOD.
- If both output
frequencies are the same, and have the same SSC settings (that
is, both use SSC or both do not use SSC), only one FOD is
required.
- If both output
frequencies are different, but have the same SSC settings, the
outputs can share an FOD to conserve current. If both
frequencies can be generated from dividing a single valid FOD
frequency by the channel divider options, then the second FOD
can be disabled. Otherwise, both FODs must be used. If both
outputs require SSC, then this frequency plan can not be
supported by the LMK3H0102-Q1 device.
- If one output
requires SSC and the other does not, then the SSC output must
use FOD0 and the non-SSC output must use FOD1.
- If SSC is being used, determine whether or not a
preconfigured down-spread modulation, a custom down-spread modulation,
or a center-spread modulation is required for the application. If a
custom configuration is required, follow the steps outlined in Spread-Spectrum Clocking.
- Set the digital clock divider such that the
digital clock frequency is as close to 50MHz as possible.
- Determine the REF_CTRL pin functionality. If this is used as an additional LVCMOS reference clock, verify that the desired frequency can be generated based on the FOD0 and FOD1 frequencies, as the divider range for the REF_CLK output is /2, /4, or /8 only.
- Keep in mind that if SSC is used on FOD0, and the REF_CLK source is FOD0, this output now has SSC as well.
- Setting the Output Formats
- The output formats that are required are based
upon the clock format needed in the system. For PCIe applications, this
is most often a 100MHz LP-HCSL clock. The internal termination
resistance value must be chosen such that the impedance matches the
input impedance of the receiver. Note that the termination scheme is
different for AC-LVDS and DC-LVDS - an AC-LVDS receiver requires an
AC-LVDS output from the LMK3H0102-Q1.
- For differential outputs, the slew rate is
selectable, from the slowest range (1.4V/ns to 2.7V/ns) to the fastest
range (2.3V/ns to 3.5V/ns).
- For LP-HCSL outputs of either termination scheme,
the amplitude is selectable between 625mV and 950mV.
- For LVCMOS outputs, the P and N phases can be in phase, opposite, or individually enabled or disabled. This allows for the generation of up to five LVCMOS clocks between OUT0, OUT1, and the REF_CTRL pin.
- For LVCMOS outputs, the VDDO_x voltage MUST match
the VDD voltage if VDD is 1.8V or 2.5V.
- Output Enable Behavior
- The output enable pin is active low by default,
with an internal pulldown resistor to GND. If this functionality is not
desired, then OE_PIN_POLARITY can be set to '0' to change the behavior
of the OE pin to active-high. If this is done, the internal pulldown is
disabled, and an internal pullup to VDD is used.
- Determine whether or not both outputs being
disabled means that the device enters low-power mode. While this is able
to conserve current, low-power mode is not recommended for any
applications where the clocks must turn back on quickly, such as PCIe
clocking.
For the PCIe example, the following settings are required:
- One FOD can be used to generate
both LP-HCSL outputs. As such, FOD0 can be set to have an output frequency of
200MHz, with Channel Divider 0 set to divide by two. Alternatively, FOD0 can be
set to 400MHz with a divider by four. Both configurations are valid. Both output
drivers select Channel Divider 0, and are both set to LP-HCSL.
- DIG_CLK_N_DIV must be set
to two to set the state machine clock properly. The state machine clock
must be as close to 50MHz as possible without exceeding this frequency.
Equation 9 shows the relationship between the digital state machine frequency,
the frequency selected by the CH0_FOD_SEL multiplexer, and the
DIG_CLK_N_DIV field. Write the DIG_CLK_N_DIV field only while the device
is in the low power state.
- FOD0 can be used to generate the
25MHz LVCMOS clock, 200MHz / 8 = 25MHz. The REF_CLK divider options are divides
by two, four, or eight. Therefore, REF_CLK_DIV must be set to 3 for achieving a
divide by 8.
Equation 9.
where FDIG is the digital
state machine clock frequency and FCH0_FOD_SEL is the frequency selected
by the CH0_FOD_SEL multiplexer