SNAU290 November 2024 LMK3H0102
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15:10 | DIG_CLK_N_DIV | R/W | 0x00 |
Digital State Machine clock rate. Derived from the FOD frequency sourced by the CH0_FOD_SEL multiplexer. The target for the frequency is 50MHz maximum. The actual divide value is the DIG_CLK_N_DIV value plus 2. This field is stored in the EFUSE. |
| 9:3 | FOD0_N_DIV | R/W | 0x10 |
Integer Ratio of BAW frequency to FOD0 frequency. This field is stored in the EFUSE. |
| 2:1 | Reserved | R | N/A |
Reserved, do not write to this field. |
| 0 | OTP_BURNT | R/WL | 0x1 | Indicates if the EFUSE has been programmed. If this field is '1', the EFUSE is programmed. |