The DP83TC814 offers
sensors for monitoring voltage at the supply pins. Undervoltage monitoring are
always active in the DP83TC814 by default. If an undervoltage condition is detected, interrupt
status flag is set in register 0x0013. These interrupts can also be optionally
routed to the INT pin using the same register.
Use the following steps to read each
sensor.
- Program register 0x0467 = 0x6004; Initial configuration of monitors
- Program register 0x046A = 0x00A3; Enable Monitors
- Configure register 0x0468 with the corresponding setting to select the required
sensor.
- VDDA Sensor: Use 0x0468 =
0x0920
- VSLEEP Sensor: Use 0x0468
= 0x1920
- VDDMAC Sensor: Use 0x0468
= 0x2920
- VDDIO Sensor: Use 0x0468
= 0x3920
- Read register 0x047B[14:7] and convert this output code to decimal.
- Use the output code in the following equations to get the absolute value of the
sensor. See the Table 7-2 table for constant values for corresponding sensors.
- vdda_value = 3.3 +
(vdda_output_code - vdda_output_mean_code) × slope_vdda_sensor
- vsleep_value = 3.3 +
(vsleep_output_code - vsleep_output_mean_code) ×
slope_vsleep_sensor
- vddmac_value = 3.3 +
(vddmac_output_code - vddmac_output_mean_code) ×
slope_vddmac_sensor
- vddio_value = 3.3 +
(vddio_output_code - vddio_output_mean_code) × slope_vddio_sensor
Table 7-2 Sensors Constant Values
| SENSOR |
CONSTANT |
VALUE |
| VDDA |
vdda_output_mean_code |
126 |
| slope_vdda_sensor |
0.0088 |
| VSLEEP |
vsleep_output_mean_code |
134 |
| slope_vsleep_sensor |
0.0088 |
| VDDMAC |
vddmac_output_mean_code |
205 |
| slope_vddmac_sensor |
0.016 |
| VDDIO |
vddio_output_mean_code |
205 |
| slope_vddio_sensor |
0.016 |