SNLU237B September 2018 – July 2025
Figure 1-3 Jumper Placements for Onboard PowerThe jumpers shown in Figure 1-3 can be used to choose whether a particular voltage rail is supplied through onboard LDOs or an external power supply. If an external power supply is desired on a voltage rail, then change the respective jumper from position 1-2 (LDO) to 2-3 (External). Then, connect the appropriate voltage on the corresponding pin to the P1 connector. For example, if the VDDA2P5 is to be supplied from an external supply, then change jumper position of J35 from 1-2 to 2-3. Then connect the 2.5-V external supply on pins 9-10 on the P1 connector. Note that pin 9 is supply and pin 10 is ground.