SPRACU5C June 2021 – September 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
AC-coupling capacitors are recommended for PCIe transmit and receive signals. Place the capacitors closer to the transmitter.
If an on-board PCIe connector is used, connect the receive signals from the processor directly to the connector. The AC-coupling capacitors for the receive signals are expected to be available on the device connected to the PCIe connector.