SPRACU5C June 2021 – September 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Connect USB0_DM and USB0_DP signals directly from the processor to the USB hub upstream port. The hub then distributes these signals to the downstream ports as needed. Ground the connector ID to enable host mode. As each hub has different implementation requirements, it is recommended to follow the hub manufacturer recommendations.
For more information on USB2.0 interface, see the [FAQ] AM6442, AM6441, AM6422, AM6421, AM6412, AM6411 Custom board hardware design – USB2.0 interface.