SPRAD05E August 2024 – October 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
For a complete list of processor power supply rails and recommended operating condition (ROC), see the Recommended Operating Conditions section in the Specifications chapter of the device-specific data sheet.
For more information about processor ROC, see the following FAQ:
The processor family does not support dynamic voltage scaling (switching) for processor core, peripheral core and peripheral analog supplies after the processor cold reset input (MCU_PORz) has been released. Some of the IO supply for IO groups support dynamic voltage switching. Refer to the IO supply for IO groups description in the device-specific data sheet for the IO supply for IO groups that support dynamic voltage switching.
For more information about dynamic voltage scaling (DVS) and dynamic frequency scaling (DFS), see the following FAQ:
The recommendation is to verify that the supplies connected to the processor supply rails are within the Recommended Operating Conditions of the device-specific data sheet.