SPRADN2 January   2025 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3519 , MSPM0L1227 , MSPM0L1228 , MSPM0L2227 , MSPM0L2228

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Nonvolatile Memory (NVM) Basic Introduction
    1. 1.1 Flash Memory Protection
  5. 2Customer Secure Code (CSC) Introduction
    1. 2.1 CSC Execution Overview
    2. 2.2 CSC Memory Maps
    3. 2.3 CSC Execution Process
  6. 3Bank Swap Example Implementation
    1. 3.1 CSC Code Project Preparation
      1. 3.1.1 Enable CSC in NONMAIN
      2. 3.1.2 Implementation of CSC Application Code - Bank Swap Feature
    2. 3.2 Application Code Project Preparation
  7. 4Common Use Case Introduction
  8. 5Data Bank Introduction
    1. 5.1 Data Bank Protection
    2. 5.2 Data Bank Erase Write Operation
  9. 6Summary
  10. 7References

Nonvolatile Memory (NVM) Basic Introduction

The nonvolatile memory system provides on-chip programmable flash memory for storing executable code and data, the device boot configuration, and parameters which are preprogrammed by TI from the factory. The NVM is organized into one or more banks, and the memory in each bank is further mapped into one or more logical memory regions and system address space for use by the application. Key flash bank terms are defined in Table 1-3 to be used as a reference for the rest of this application note.

Table 1-1 NVM System Terminology
Term Definition Size
Flash word Basic data size for program and read operations on the flash memory (also the read bus width to the system) 64 data bits (72 bits with ECC)
Word line Group of flash words within a sector, with maximum program operation limit before sector erase 16 flash words (128 data bytes, optionally 16 ECC bytes)
Sector Group of word lines that are erased together (minimum erase resolution of the flash memory) 8 word lines (1024 data bytes, optionally 128 ECC bytes)
Bank Group of sectors that can be mass erased in one operation. Only one read, program, erase, or verify operation can run concurrently on a given bank. Variable

The NVM system on MSPM0 device provides support for up to 5 flash memory banks (enumerated as BANK0 through BANK4). The number of flash banks present is device dependent. To determine the bank scheme of a particular device, review the detailed description section of the specific device data sheet Flash Memory chapter.

Within a given flash bank, an ongoing program or erase operation stalls all read requests to that bank until the operation has completed and the flash controller has released control of the bank. On devices with more than one flash bank, read request to other flash banks are unaffected by operations in a different flash bank. As such, the presence of multiple banks improves performance in application cases such as:

  • Live firmware updates - an application can continue to execute code functions out of one flash bank while a new image is written to a separate flash bank.
  • Data Logging and EEPROM emulation: an application can continue to execute while writing data to a separate bank.
  • The memory within each bank is mapped to one or more logical regions based upon the functions that the memory in each bank supports. There are three regions: FACTORY, NONMAIN (Configuration NVM) and MAIN. Some devices also have a independent DATA bank which can be used as data saving or EEPROM emulation. The DATA bank is further detailed in Section 5.
Table 1-2 Flash Memory Regions
Flash Memory Region Region Contents Executable Used by Programmed by
FACTORY Device ID and other parameters No Application TI only (not modifiable)
NONMAIN (Configuration NVM) Device boot configuration (BCR and BSL) No Boot ROM TI, User
MAIN (Flash Memory) Application code and data Yes Application User

Devices with one bank implement the FACTORY, NONMAIN, and MAIN regions on BANK0 (the only bank present), and the DATA bank is not available. Devices with multiple banks also implement FACTORY, NONMAIN, and MAIN regions on BANK0, but include additional banks (BANK1 through BANK4) that can implement MAIN or DATA bank.

Note:

Operating on a NVM

Any interruption during the erase or re-program operations (that is, unplugging device, removing SWD jumpers, hitting reset by accident, canceling the code download, an IDE crash, and so forth) can brick the device permanently. Improper configuration of NONMAIN can also lead to permanent locking of the device.

 Memory Organization Example -
                    Single Bank Configuration Figure 1-1 Memory Organization Example - Single Bank Configuration

Figure 1-2 is an example of a three bank configuration with a 512KB MAIN region split across BANK0 and BANK1, with a 16KB DATA bank provided in BANK2. Like the single bank example, NONMAIN and FACTORY regions are included in BANK0. This example supports EEPROM emulation in the DATA bank without stalling fetches to MAIN, and also supports dual-image applications where BANK0 main can be written to without stalling fetches to BANK1 main (and the reverse). Most devices with a main region ≥256KB in size implement some form of multibank configuration.

 Memory Organization Example -
                    Multiple Bank Configuration Figure 1-2 Memory Organization Example - Multiple Bank Configuration

For multi bank devices, the BANK0 and BANK1 are considered as Physical Bank 0 (PB0) and Physical Bank 1 (PB1). These banks can switch addresses depending on the bank swap configuration, but upon a BOOTRST the entry point is always PB0.

For example, the Logical Bank 0 (LB0) always maps to address 0x0000.0000 - 0x0003.FFFF, and Logical Bank 1 (LB1) maps to 0x0004.0000 - 0x0007.FFFF. The two logical banks can map to either PB0 or PB1.

Further sections focus on how to take advantage of multiple banks features to achieve application requirements.