SPRADS3 July 2025 AM62P
This application note serves as a technical guide for configuring the display subsystem of the system, providing engineers with the required guidelines to drive one or more display panels simultaneously.
The document details the operational modes and performance capabilities for the three primary display interfaces. The document explains how each interface can be set up in various ways, offering a different balance between support for high-resolution screens and the ability to run multiple displays.
A key focus of this application note is to clarify the rules and limitations when using several displays at the same time. The document highlights different permutations of DSS-specific resource allocation, making sure designers can make informed choices to achieve a stable and functional multidisplay setup that meets application specific requirements.
For getting help in debugging display-related issues, see this Debug Guide and then post queries on e2e.ti.com if the issue still persists.