SPRADT4 July 2025 TMS320F28388D , TMS320F28388S
This document was translated from a simplified Chinese source. (ZHCAFM7)
In multi-core processor systems, the timeliness and accuracy of data transfers between cores are critical for realizing real-time control systems. In the 2838xD device, the absence of shared RAM space between CPU2 and CPU1.CLA1 poses a challenge for achieving fast data interaction between them. This paper analyzes the limitations of conventional IPC-based data transfer methods and, by leveraging the existing peripheral resources of the 28388D, proposes an "IO trigger + DMA transfer" approach to enable real-time, high-speed data interaction between CPU2 and CPU1.CLA1. Furthermore, this method is also applicable to processors with architectures similar to the 2838xD, such as the F28P65, facilitating fast inter-core data interaction in multi-core processors.