SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
The interface register sets control the CPU read and write accesses to the Message RAM. There are two interface register sets for read and write access (IF1 and IF2) and one Interface Register Set for read access only (IF3).
Due to the structure of the Message RAM, it is not possible to change single bits or bytes of a message object. Instead, always a complete message object in the Message RAM is accessed. Therefore the data transfer from the IF1/IF2 registers to the Message RAM requires the message handler to perform a read-modifyÂwrite cycle. First those parts of the message object that are not to be changed are read from the Message RAM into the Interface Register set, and after the update the whole content of the Interface Register set is written into the message object.
After the partial write of a message object, those parts of the Interface Register set that are not selected in the Command Register are set to the actual contents of the selected message object. After the partial read of a message object, those parts of the Interface Register set that are not selected in the Command Register are left unchanged.
By buffering the data to be transferred, the Interface Register sets avoid conflicts between concurrent CPU accesses to the Message RAM and CAN message reception and transmission. A complete message object (see Section 21.13.1) or parts of the message object can be transferred between the Message RAM and the IF1/IF2 Register set in one single transfer. This transfer, performed in parallel on all selected parts of the message object, maintains the data consistency of the CAN message.
There is one condition that can cause a write access to the message RAM to be lost. If MsgVal = 1 for the message object that is accessed and CAN communication is ongoing, a transfer from the IFx register to message RAM can be lost. The reason this can happen is that the IFx register write to the message RAM occurs in between a read-modify-write access of the Host Message Handler when in the process of receiving a message for the same message object.
To avoid this issue with receive mail boxes, reset MsgVal before changing any of the following: Id28-0, Xtd, Dir, DLC3-0, RxIE, TxIE, RmtEn, EoB, Umask, Msk28-0, MXtd, and MDir.
To avoid this issue with transmit mail boxes, reset MsgVal before changing any of the following: Dir, RxIE, TxIE, RmtEn, EoB, Umask, Msk28-0, MXtd, and MDir. Other fields not listed above, like Data, can be changed without fear of losing a write to the message RAM.