SPRUI78D March 2019 – January 2022 F28377D-SEP , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
During the device boot, it goes through various phases as indicated in Figure 4-10. In the pre-operational phase (before starting the application), the application code is expected to perform a set of checks to ensure correct initialization of device security which includes checks to confirm correct link-pointer settings, CRC lock setting, correct partitioning of secure RAM blocks and Flash sectors (Grab Bits), setting for execute only protection for secure RAM blocks and Flash sectors, correct partitioning of the CLA and Flash Bank2 and correct settings for boot configuration. Before starting the execution of downloaded code user should check the integrity of the code using CRC function. Once pre-operational checks are successfully completed with expected results, the device can enter the application phase.