SPRUIT1B May 2020 – November 2020
There are six LIN interfaces present in the GESI Expansion Board (3x Dual Port LIN). A Dual pin Switch (SW2, SW3 and SW4) is provided for each LIN Port to select the mode of Corresponding LIN Port as a Slave or Master. To set the LIN port as Master CLOSE the corresponding Switch and to set LIN ports as Slave OPEN the Corresponding Switch.
Figure 4-7 Dual Port LIN Interface