SPRUJ85A April 2024 – August 2024
PRODUCTION DATA
It has been found that few EVMs when connected to the PC and connect through Code Composer Studio(CCS), the user is prompted to update the firmware as per below window. Upon clicking on Update button, the update is unsuccessful and CCS just disconnects from the board and the board is no longer detected by CCS. This has been mostly observed with CCS versions 12.4 and above.
Figure 4-2 CCS prompt to update
firmwareThe below are the steps of recovering a board when CCS fails to detect the board as mentioned above.
The failure to detect the board is mostly attributed to the wrong firmware version on the XDS110 debugger on the board. Thus the XDS110 debugger would need to be re-flashed with the latest firmware available with the CCS on the user's PC. Follow the below steps to do the same.
Figure 4-3 Location of Pins
64 and 97 on U24
Figure 4-4 XDS110 Firmware update
commands in Command PromptPost the above steps are complete, CCS should be able to detect and connect to the XDS110 debugger on LP-AM263P.
More details about XDS110 firmware and updating it can be found in https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds110.html#manual-update