SPRZ457H January 2021 – December 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
DDR: Valid stop value must be defined for write DQ VREF training
The DDR PHY uses start, stop, and step-size values for write DQ VREF training. If the stop value is not equal to the start value + a multiple of the step-size, then the final VREF setting can go beyond the maximum VREF range, causing the training to hang.
Program the stop value as follows:
PI_WDQLVL_VREF_INITIAL_STOP = (multiple of PI_WDQLVL_VREF_INITIAL_STEPSIZE) + PI_WDQLVL_VREF_INITIAL_START
This workaround is implemented in the DDR Subsystem Register Configuration Tool v0.03.00 or later. See https://dev.ti.com/sysconfig for more details.