SPRZ457H January   2021  – December 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2287
      2.      i2351
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2103
      4.      i2184
      5.      i2189
      6.      i2236
      7.      i2185
      8.      i2196
      9.      i2207
      10.      i2208
      11.      i2228
      12.      i2232
      13.      i2244
      14.      i2245
      15.      i2091
      16.      i2235
      17.      i2303
      18.      i2317
      19.      i2134
      20.      i2257
      21.      i2277
      22.      i2285
      23.      i2310
      24.      i2311
      25.      i2313
      26.      i2328
      27.      i2241
      28.      i2279
      29.      i2307
      30.      i2320
      31.      i2329
      32.      i2331
      33.      i2243
      34.      i2249
      35.      i2256
      36.      i2274
      37.      i2278
      38.      i2306
      39.      i2363
      40.      i2312
      41.      i2371
      42.      i2366
      43.      i2138
      44.      i2253
      45.      i2259
      46.      i2283
      47.      i2305
      48.      i2326
      49.      i2368
      50.      i2383
      51.      i2401
      52.      i2409
  4.   Trademarks
  5.   Revision History

i2287

Package Pin Assignment Difference between SR1.0 and SR2.0

Details

Two package terminals will be assigned new signal functions as the device transitions from Silicon Revision 1.0 (SR1.0) to Silicon Revision 2.0 (SR2.0).

  • J15
    • SR1.0: Assigned to VDDS_MMC0 (MMC0 PHY IO supply). ADC0_REFP is internally connected to VDDA_ADC0
    • SR2.0: Assigned to ADC0_REFP (ADC0 positive reference).
  • J16
    • SR1.0: Assigned to VSS (Ground). ADC0_REFN is internally connected to VSS
    • SR2.0: Assigned to ADC0_REFN (ADC Negative Reference)
Here is the guidance on using SR2.0 devices on existing boards, and recommendations for new board designs.

  • When installing SR2.0 device on existing SR1.0 designed boards
    • For boards with VDDA_ADC0 and VDDS_MMC0 connected to the same power supply
      • An SR2.0 device may experience reduced ADC0 performance
        • This can occur because ADC0_REFP will be connected to the VDDS_MMC0 digital supply which will couple noise directly into ADC0 reference.
    • For boards with VDDA_ADC0 and VDDS_MMC0 connected to different power supplies
      • Potential applied to VDDS_MMC0 must never exceed the potential applied to VDDA_ADC0.
        • This condition of operation is required because the new SR2.0 pin assignment connects ADC0_REFP to the VDDS_MMC0 digital power supply and the internal ESD protection circuit associated with ADC0_REFP is referenced to VDDA_ADC0, which may be sourced from a separate analog power supply. This requires the potential applied to ADC0_REFP to be less than or equal to potential applied to VDDA_ADC0. This power sequencing requirement for ADC0_REFP relative to VDDA_ADC0 is passed along to VDDS_MMC0 when a SR2.0 device is installed on a PCB previously designed for a SR1.0 device. Therefore, it is important to confirm this condition of operation is not violated during power-up and power-down when VDDS_MMC0 and VDDA_ADC0 are sourced from different power supplies.
      • If ADC0 is not being used, where VDDA_ADC0 is connected to VSS as described in the Connections for Unused Pins section of the datasheet, a SR2.0 device cannot be installed
        • This is not allowed because the potential applied to ADC0_REFP can never exceed the potential applied to VDDA_ADC0, and ADC0_REFP will be connected to VDDS_MMC0 when a SR2.0 device is installed on a PCB previously designed for a SR1.0 device.
  • New board design which will support both SR1.0 and SR2.0 devices
    • Place a zero ohm resistor on the back-side of the PCB, under the BGA array, connected between J13 and J15.
      • When SR1.0 is installed, do not populate this resistor
      • When SR2.0 is installed, populate this resistor.
    • An additional high-frequency de-coupling capacitor should be placed on the back-side of the PCB, under the BGA array, connected between J15 and J16.
    • Connect J16 directly to VSS power plane
  • New board design which will only support SR2.0 devices
    • Connect J13 to J15
    • Connect J16 directly to VSS power plane
    • An additional high-frequency de-coupling capacitor should be placed on the back-side of the PCB, under the BGA array, connected between J15 and J16.
    • See Note
Note: A SR1.0 device should not be installed on a PCB only designed to support SR2.0 devices. This PCB would connect J13 and J15 to the ADC0 analog power supply, and installing a SR1.0 device that internally connects J15 to K14 would short the VDDA_ADC0 analog power supply to the VDDS_MMC0 digital power supply.