SWRA493A October 2015 – October 2026 CC1101 , CC110L , CC1120 , CC1121 , CC1125 , CC1190 , MSP430F5438A
A common issue with developing a new system from start based on transceivers is how to test the various parts of the system either by themselves or as part of the entire system.
Texas Instruments provides a very powerful and comprehensive tool called SmartRF™ Studio 7, which enables testing of all our devices; however, in some cases, the hardware requirements for the system to operate may not be available or using a PC may not be the preferred way to performing testing.
The software described in this application report provides a simple alternative in these use cases. The software is based on basic drivers already developed for MSP430’s to implement a simple UART-based test system.
The software discussed in this document can be downloaded from the following URL: http://www.ti.com/lit/zip/swra493.