SWRA493A October 2015 – October 2026 CC1101 , CC110L , CC1120 , CC1121 , CC1125 , CC1190 , MSP430F5438A
This command starts a third special test mode that forces the device into RX at a specified frequency; choose the frequency by selecting a channel starting from 0. The value 0 produces a frequency at the base frequency currently configured in Section 1.10.
Static RX (RX leakage test) (line, chan), for example,(3 25)This command is enabled by entering 3 followed by the desired channel number for this test. For details on base frequency and channel spacing configuration, see Section 1.10. To exit test mode, see Section 1.1.