The boot process consists of two
consecutive steps: primary or ROM boot loader (RBL) process, followed by the
secondary boot loader (SBL) process. As soon as the EVM is powered ON, the ROM
bootloader or RBL starts running. The RBL is the primary bootloader. The goal of RBL
is to load, verify, optionally decrypt, and launch authentic the R5F software image
that accomplishes secure boot goals (in a secure variant). The RBL process is
implemented jointly by the R5F and HSM ROM as illustrated in Figure 3-3. The RBL
expects the image (SBL in this case) to always be signed.
Note: Please note that the C66 Run time and C66 Core is not applicable for
AWR2544.
At high level the boot flow can be explained as below.
- The HSM ROM is the first code to
be executed at system reset. HSM ROM executes a set of self-tests for data SRAM,
program SRAM, ROM code integrity, as part of device initialization and
configures the APLL. HSM ROM also releases the R5F from reset.
- In the HSM, ROM PBIST is
performed on secure RAM, public RAM and ROM code integrity check is performed
for the HSM sub system.
- In the R5F RBL, PBIST is
performed on MSS TCMA,MSS TCMB and MSS_L2 memories.
- The R5F checks for the SOP
settings and based on continued execution.
- In the UART boot mode or Flashing
mode, the RBL is expected to get flash programmer (or any other relevant image)
from UART. The flash programmer is generally used to download and flash the SBL
to the QSPI flash.
- In the QSPI boot mode or
Functional mode, the RBL loads the SBL from the flash memory on to the internal
RAM and begins execution.
Note: Please note for AWR2544 device the
RBL does not perform the PBIST on MSS TCM memories and MSS L2. The user is required
to perform the operation in the SBL. Please check the AWR2544 SDK for this
implementation.
Note: Please note for AWR2x44P device the RBL does not perform
PBIST on secure RAM.
Key points
- The ROM bootloader loads only one
image and to R5F L2 RAM only.
- The ROM bootloader sets up the
root clock by starting the APLL. The root clock is at 200MHz.