In functional mode, the bootloading of
an image from the SDF is the first bootmode attempted by the bootloader. This
bootmode involves the following steps:
- Pinmux the QSPI pins of the
AWR294x device:
- QSPI[0]: Ball U11
- QSPI[1]: Ball V11
- QSPI[2]: Ball T11
- QSPI_CLK: Ball R10
- QSPI_CS: Ball U12
- Pinmux the QSPI pins of the
AWR2x44P device:
- QSPI[0]: Ball P2
- QSPI[1]: Ball N2
- QSPI[2]: Ball P1
- QSPI_CLK: Ball R2
- QSPI_CS: Ball T1
- QSPI is set up to operate at
80MHz for AWR294X, AWR2x44P device and 75MHz for AWR2544 device.
- The sFLASH discoverable
parameters (SFDP) command is issued to retrieve the JEDEC compliant response,
which includes information regarding the sFLASH capabilities and command set.
When the SFDP response is received, the information is used to communicate with
the SDF and further interpret the contents and load the images. For more
information on the flash variants supported with AWR294x, AWR2x44P, AWR2544
devices, refer to Flash Variants Supported by the mmWave Sensor application note.
Note: Please note that the CAN interface
is not applicable for AWR2544 device.
Key points
- The RBL performs the read from
the SDF, based on the highest capability mode (quad, dual, or single) as
published by the SDF in response to the SFDP command.
- For SDF variants that support
quad mode, the quad mode commands are issued; if the quad enable (QE) bit is not
set, the communication fails. In such cases, the load flow assumes that the QE
bit in the SDF is already set.
- SBL is user implemented entity
which has logic to achieve above mentioned flow. SBL can use any interface out
of UART, CANFD or Ethernet if required.
- Fallback images: the RBL supports
loading of images from the following locations only as a fallback Mechanism, if
one of the images is corrupted in the SDF. The locations of the images are:
- – META IMG1(SDF offset –
0x0)
- – META IMG2(SDF offset –
0x40000)