SWRA814 May 2024 CC1311P3 , CC1311R3 , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC1354P10 , CC1354R10
This document details hardware change considerations when migrating between different devices within the CC131x and CC135x family of SimpleLinkā¢ wireless MCUs. The changes are because of different physical properties of the devices, such as package sizes, and because of updated reference designs that utilize improved technologies like smaller passive component package sizes. The hardware changes can be optional or mandatory depending on the specific device-to-device migration. This document provides advice on when a change is required or recommended.
Section 2 provides a reference guide for the differences between the CC131x and CC135x family of devices and highlights other useful TI documentation when appropriate. Section 3 details the necessary changes for migrating between different members of the device family, with references to Section 2 for more specific information. Section 5 provides links to recommended TI source documentation, additional TI support resources, and the data sheets for the CC131x and CC135x devices.