SWRU635 May   2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Temperature Range
    3. 2.3 Energy Trace
    4. 2.4 Hardware and Debug Setup
      1. 2.4.1 Using a LaunchPad XDS110 Debug Probe
      2. 2.4.2 Using a Generic XDS110 Debug Probe, Including a Separate LaunchPad
    5. 2.5 BoosterPack Connector Pinout
    6. 2.6 XDS110 Interface Connector
    7. 2.7 Debug Interface Connector
    8. 2.8 Jumper Information
    9. 2.9 Push Buttons
  9. 3Advanced Use of the LaunchPad Hardware
    1. 3.1 External Antenna
    2. 3.2 XDS110 GPIOs
    3. 3.3 Reset Selection on BoosterPack Connector
    4. 3.4 I2C Pullup Resistors
  10. 4Software
    1. 4.1 Getting Started
    2. 4.2 Out of Box Demo
  11. 5Hardware Design Files
    1. 5.1 Reference Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Compliance Information
    1. 6.1 CE Compliance
    2. 6.2 REACH Compliance
    3. 6.3 Waste Electrical and Electronic Equipment (WEEE) Compliance
  13. 7Additional Information
    1. 7.1 Trademarks
  14. 8References

Out of Box Demo

The LP-EM-CC2745R10-Q1 is preprogrammed with the Data Stream Application software that allows wireless communication with smartphones and tablets over Bluetooth Low Energy. Simply connect the LP-EM-CC2745R10-Q1 to the XDS110 Debug Probe and then to a computer or power supply.

When power is applied, the board will run a power-on self-test and the green LED will be lit.

To test the functionality of the Data Stream Application, download the SimpleLink Connect application from one of the two App Stores below:

This app lets you control and visualize the Data Stream demo software running on the LaunchPad. An example of the Data Stream Application is shown in Figure 4-1.

LP-EM-CC2745R10-Q1 Data Stream Application SW ExampleFigure 4-1 Data Stream Application SW Example

The Data Stream Application status information can also be seen on the UART port of the host PC, as shown in Figure 4-2.

LP-EM-CC2745R10-Q1 Data Stream Application Status ExampleFigure 4-2 Data Stream Application Status Example

Important: Clear your phone or tablet’s Bluetooth cache before running the application or when changing the application on the CC2745R10-Q1. If this step is not performed, then you may not see the available characteristics in the smartphone app. Note that closing the smartphone app or rebooting your phone does NOT clear the Bluetooth cache.

iOS: This is accomplished by toggling Bluetooth Off then On through either the Settings → Bluetooth menu or the Control Center (Bluetooth icon).

Android: The procedure can vary by make, model, and software version. On recent versions, navigate to Settings → Apps Scroll over to All → Choose Bluetooth Share and tap on Clear Cache.