The LP-EM-CC2745R10-Q1 has two user-configurable push buttons as shown in Figure 2-1:
- BTN-1 is connected to DIO20 of the
CC2745R10-Q1. This is also directly connected to the BoosterPack header J1:30.
- BTN-2 is connected to DIO0 of the
CC2745R10-Q1. This is also directly connected to the BoosterPack header J2:40.