SWRZ150A December 2024 – October 2025 AWR2544
Spurs Caused due to Digital Activity
AWR2544
Digital filtering activity can potentially couple to analog circuits leading to spurs in the LO, which may also be seen in the Rx data. Such a spur in the Rx data would be seen at the spur frequency offset around a strong object.
Following are the different spurs that can potentially be observed:
[Fs=Profile Sampling Rate]
The user should avoid sampling rates in the range mentioned above or use exactly the center of the sampling rate range (so that spur is at 0 Hz).