SWRZ171 July 2025 CC2755P10 , CC2755R10
Spurious temperature update interrupts from BATMON in standby.
When using PMUD.EVENT.TEMP_OVER_UL or PMUD.EVENT.TEMP_BELOW_LL as wake-up interrupts, these are the other settings that have to be enabled:
Select GLDO as the source for VDDR regulation by setting PMCTL.VDDRCTL.SELECT to 0x0.
This causes a slight increase in standby power consumption. Please check the ‘Power Consumption – Power Modes’ section of the data sheet for exact details.
Set SYS0.TMUTE4.RECHCOMPREFLVL to 0x2
Set SYS0.TMUTE5.GLDOISSET to 0x1E
This workaround would be incorporated into future releases of SimpleLink™ Low Power F3 software development kit (SDK).