TIDUDA6A December   2017  – January 2022

 

  1.   Description
  2.   Resources
  3.   Features
  4.   Applications
  5.   5
  6. 1 System Description
    1. 1.1 Key System Specifications
  7. 2 System Overview
    1. 2.1 Block Diagram
    2. 2.2 System-Level Description
    3. 2.3 Highlighted Products
      1. 2.3.1 Analog Signal Chain
        1. 2.3.1.1 LMH5401
        2. 2.3.1.2 LHM6401
        3. 2.3.1.3 BUF802
      2. 2.3.2 Clock
        1. 2.3.2.1 LMK61E2
        2. 2.3.2.2 LMK04828
        3. 2.3.2.3 LMX2594
      3. 2.3.3 Power
        1. 2.3.3.1 TPS82130
        2. 2.3.3.2 TPS7A84
    4. 2.4 System Design Theory
      1. 2.4.1 High-Speed, Low-Phase Noise Clock Generation
      2. 2.4.2 Channel-to-Channel Skew
      3. 2.4.3 Deterministic Latency
        1. 2.4.3.1 Importance of Deterministic Latency
      4. 2.4.4 Analog Front End
      5. 2.4.5 Multichannel System Power Requirement
      6. 2.4.6 Hardware Programming
  8. 3 Circuit Design
    1. 3.1 Analog Input Front End
      1. 3.1.1 High-Input Impedance Buffer Implementation Using the BUF802
    2. 3.2 High-Speed Multichannel Clocking
    3. 3.3 Power Supply Section
      1. 3.3.1 DC-DC
        1. 3.3.1.1 How to Set 2.1-V Output Voltage
      2. 3.3.2 LDOs
  9. 4 Host Interface
  10. 5 Hardware Functional Block
  11. 6 Getting Started Application GUI
  12. 7 Testing and Results
    1. 7.1 Test Setup and Test Plan
    2.     44
    3. 7.2 SNR Measurement Test
    4. 7.3 Channel-to-Channel Skew Measurement Test
    5. 7.4 Performance Test Result
    6. 7.5 Multichannel Skew Measurement
    7. 7.6 49
  13. 8 Design Files
    1. 8.1 Schematics
    2. 8.2 Bill of Materials
    3. 8.3 Altium Project
    4. 8.4 Gerber Files
    5. 8.5 Assembly Drawings
  14. 9 Software Files
  15. 10Related Documentation
    1. 10.1 Trademarks
  16. 11About the Authors
    1. 11.1 Acknowledgment
  17. 12Revision History

High-Input Impedance Buffer Implementation Using the BUF802

This reference design focuses on design of an analog front end with 50-Ω input as previously discussed, however in some use cases like that of DSO it is often desired to have a capability of a high-input impedance input to the tune of 1 MΩ. BUF802 helps implement this requirement by use of a JFET input unity gain buffer.

Data acquisition systems that require a high-input impedance mode usually follow one of two approaches; a custom front-end ASIC or a discrete JFET implementation. Either of these approaches incur either a high cost of developing and manufacturing a custom ASIC or a complex discrete circuit that comes with its own set of design challenges. The BUF802 provides a single chip alternative to both ASIC and FET-based implementations by providing an all-in-one solution that provides a simpler and more cost-effective solution without sacrificing performance.

Figure 3-2 Discrete JFET Architecture

The typical discrete implementation, Figure 3-2, uses a precision amplifier and a discrete JFET configured in a composite loop. The purpose of the composite loop architecture is to split the input signal into low- and high-frequency signal paths, pushing through two different circuits and recombining them at the output. One of the main challenges with the composite loop architecture shown in Figure 3-3 is achieving smooth interleaving of the two paths to ensure a flat frequency response. Any mismatch in the transfer function of the two paths leads to discontinuity in the net transfer function frequency response resulting in a loss of signal fidelity, see Figure 3-3.

Figure 3-3 Crossover Frequency Region

Additional drawbacks with implementing a discrete design include, but are not limited to: dealing with a complex system response, higher supply rails, component and channel mismatch, additional compensating for input and output protection. For a more in-depth look on discrete design challenges and how the BUF802 helps overcome these problems, see the Simplify analog front-end designs with Hi-Z buffersE2E™ forum.

Figure 3-4 TIDA-01022 Analog Front End

Figure 3-4 shows the TIDA-01022 fully differential AFE that is configured for a 1.5-GHz BW (bandwidth) application and a 50-Ω input impedance. In the default configuration the AFE cannot be used to achieve high-Z mode for lower frequencies. By implementing the BUF802 composite loop at the beginning of the AFE signal chain, the functionality of a high-input impedance mode can be added.

Figure 3-5 Analog Front End With BUF802

Figure 3-5 features a 1-GHz front-end design incorporating the BUF802 to the existing reference design. Adding the BUF802 into the signal chain provides the system with a high input impedance of 50 GΩ || 2.4 pF, while maintaining the performance of the original design up to 1 GHz. The ability to switch between high-Z and 50-Ω impedance mode is achieved with a switch or relay at the input.

Using the BUF802 EVM and the TIDA-01022 hardware, the performance of the signal chain with and without the BUF802 can be measured. Figure 3-6 through Figure 3-8 show different performance metrics.

Figure 3-6 Frequency Response Comparison
Figure 3-7 Signal-to-Noise Ration (SNR) vs Frequency
Figure 3-8 Total Harmonic Distortion (THD) vs Frequency