TIDUF00 November 2021
| PARAMETER | SPECIFICATIONS SHORT RANGE | SPECIFICATIONS ULTRA-SHORT RANGE | DETAILS |
|---|---|---|---|
| Maximum range | 55 m | 10 m | This represents the maximum distance that the radar can detect an object, representing an RCS of approximately 10 m2. |
| Range resolution | 0.43m | 0.076m | This is the ability of a radar system to distinguish between two or more targets on the same bearing, but at different ranges. |
| Maximum velocity | 9.6 m/s | 7.05 m/s | This is the native maximum velocity obtained using a two-dimensional FFT on the frame data. This specification will be improved over time by showing how higher-level algorithms can extend the maximum measurable velocity beyond this limit. |
| Velocity resolution | 0.149 m/s | 0.1 m/s | This parameter represents the capability of the radar sensor to distinguish between two or more objects at the same range, but moving with different velocities. |