TIDUF89 September 2024
While a good detection system has all three of these qualities (low power, long range, low false alarm rate), the recommendation is to prioritize some over others in specific scenarios to extract the best overall system performance. The IWRL6432AOP navigates this balance by using multiple detection modes. This design guide assumes that three modes are used, but the logic can apply for two modes, or even more than three modes if necessary.
First pass mode is the default option for the radar. In first pass mode, the IWRL6432AOP operates in the lowest possible power configuration while still maintaining the ability to detect at long ranges. IWRL6432AOP does have some false alarms, even in low-noise conditions to achieve long range at the lowest possible power. For best results, the first pass mode need to be as low-power as possible, even at the expense of some false alarms.
When detections occur in first pass mode, the radar switches to second pass mode, which uses a higher-power chirp that reduces the false alarm rate of the radar, and achieves the same detection range as the first pass mode. There is no advantage for the second pass mode to detect objects at further ranges than the first pass mode, since the first pass mode is what triggers the second pass mode. The second pass mode do not have nearly as many false alarms as the first pass mode, but is acceptable to still wake up sometimes from winds, bushes and trees.
Finally, a third pass mode can be used to eliminate any false positives still detected in second pass mode. The third pass mode cannot have any false alarms if possible, since the third pass mode can be used to awaken the camera, which can draw 10-100 times more power than the radar.
By cycling between the three power modes, the IWRL6432AOP is able to take advantage of the lowest-power consumption of the first pass mode when there is very little ambient motion, while also benefiting from the minimal false alarm rate of the third pass mode. The second pass mode serves to make sure that in times of high ambient movement in the scene, when first pass mode can be too sensitive to be effective, the radar still has a reasonably low power mode.
| First Pass Mode | Second Pass Mode | Third Pass Mode | |
|---|---|---|---|
| Power Consumption | Low | Medium | High |
| False Alarm Rate | High, even in low-movement scenarios | Moderate, only when there is wind, trees, or bushes | Low |
| Detection Range | Equal | Equal | Equal |
| Percent of Time Spent in Mode | High | Medium | Small |