TIDUF89 September 2024
This test occurs in a large empty space, which can be a parking lot, open field, or a large room. Mount the radar and test setup securely to prevent the equipment from moving in the wind. Note the percentage of time spent in each mode, and the number of times the radar falsely awakens the camera.
Figure 3-5 False Alarm Rate Test - Empty
SceneThe False Alarm screen in the Industrial Visualizer displays the relevant information in the table on the bottom. The shading on the top indicates the proportion of the false alarms that originate from that region (more red = higher percentage of false alarms).

Testing performance in more crowded environments can lead to more false alarms. TI has found that a combination of velocity, SNR and height filters work particularly effectively in denser scenes.