To test the robustness of the wireless
BMS network, measure the two network key performance indicator (KPI) parameters. The
definitions are as follows:
- Path Stability (PS): Path
stability is the percentage of first time successfully received packets at each
WD node divided by the total number of packets transmitted by the WM node.
- Metric: PS >
85%
- Note: Number of
packets must be > 10000
- Packet Delivery Rate
(PDR): PDR is the percentage of packets successfully received at each WD
node divided by the total number of packets transmitted by the WM node. This
includes retransmissions needed within the 100ms interval.
- Metric: PDR >
99.9%
- Note: Number of
packets must be > 10000
The three KPI are calculated from the
data read by the statistic commands in the wBMS SDK. Calculate PDR of the node n
using Equation 3.
Equation 1.
where
- n is the number of WD nodes
Calculate PS of node n using Equation 3.
Equation 2.
where
- NumTxActualPackets is
calculated based on NumTxSuccessPackets plus the maximum number of
retries for all WD nodes during each transmission
- NumTxActualPackets
indicates the actual number of TX packets sent from RF physical layer
The PS and PDR test results of 30000
packets is shown in Table 3-6. The test
results show good network robustness of this setup for 416s cells.
Table 3-6 PS and PDR Test
Results
| NODE |
WD0 |
WD1 |
WD2 |
WD3 |
WD4 |
WD5 |
WD6 |
WD7 |
| NumTxSuccessPackets |
30001 |
| NumTxActualPackets |
33095 |
| NumRxMissedPackets |
0 |
0 |
0 |
0 |
0 |
0 |
0 |
1 |
| Retry |
225 |
710 |
560 |
643 |
465 |
341 |
609 |
1396 |
| PDR |
100% |
100% |
100% |
100% |
100% |
100% |
100% |
99.997% |
| PS |
99.320% |
97.855% |
98.308% |
98.057% |
98.595% |
98.970% |
98.160% |
95.782% |