SNAS783C June 2020 – February 2021 LMX2820
PRODUCTION DATA
The fractional modulator order is programmable and has an impact on spurs. Theoretically, the higher order the fractional modulator order, the more it pushes the lower frequency spur energy to higher frequency. However, higher order modulators add more noise and increase the minimum N divide ratio. Modulator orders higher than one can create sub-fractional spurs, depending on the value of FDEN, which is the value of the denominator of the fraction PLL_NUM / PLL_DEN, after it is reduced to the lowest terms.
MASH_ORDER | WHEN TO USE |
---|---|
Integer Mode | Integer mode (MASH_ORDER = 0) is good when the fractional circuitry is not needed. It has the advantage that it allows the lowest N divider value. Be aware that the output phase cannot be shifted with MASH_SEED in integer mode. |
1st Order Modulator | The first order modulator is good for situations where the fractional denominator is small. Theoretically, if FDEN < 7, then all the fractional spurs will be lowest with the first order modulator. If the fraction is divisible by 2, then there will be sub-fractional spurs which one has to trade-off with the primary spur level. If the primary fractional spur at offset of fPD / FDEN is far outside the loop bandwidth, this is often a good choice. |
2nd Order Modulator | The second order modulator gives good spurs. If FDEN is odd, then there are no sub-fractional spurs, so situations where FDEN > 8 and FDEN is odd, this might make sense. If FDEN is very large, like 1000000, then the fraction is likely well-randomized and one might consider a third-order modulator, if it does not overly restrict the N divider value. |
3rd Order Modulator | The third-order modulator is a good general purpose starting point if FDEN > 9 and FDEN is not divisible by 3. |