JAJSJ13B may 2020 – november 2020 TPS3703
PRODUCTION DATA
The TPS3703 is immune to short voltage transient spikes on the input pins. Sensitivity to transients depends on both transient duration and overdrive (amplitude) of the transient.
Overdrive is defined by how much the VSENSE exceeds the specified threshold, and is important to know because the smaller the overdrive, the slower the response of the outputs (RESET). Threshold overdrive is calculated as a percent of the threshold in question, as shown in Equation 7:
where: