Use the following steps for I2C
communication verification. Assuming the jumper settings in Table 3-2 have been followed, the I2C address for U1 is 0x65, and the
I2C address for U2 is 0x67. If R29 and R32 have been populated, then the
I2C address for U4 is 0x6B.
- In BQStudio, click Field View and select the I2C address
for U1 (0x65).
- Click Read Register at the top of the page. Device ACK OK
appears at the top right.
- Verify that VAC1 and VOUT are reported as Present.
- Change the following register settings:
- Disable the watchdog timer
- Set VAC1 OVP to 10.5 V or higher
- Click Read Register again. In addition to VAC1 and VOUT, VBUS is
also reported as Present.
- Measure → VVBUS_M-GND(TP2
and TP37) = 8.3 ± 0.2 V