SLWU087E november 2013 – june 2023
Located in the lower left corner of the GUI is an I/Q Multi-tone Generator tool that allows the user to generate test patterns that can be used with the HSDC Pro GUI. The following parameters are used with this tool:
Tone BW – Tone bandwidth in Hertz. For Megahertz, enter a "M" after the number.
# – Number of tones. If set to 1, Tone BW will be ignored.
Tone Center – Center frequency of tones in Hertz.
# of Samples – Number of test samples. 4096 to 2M, in increments of 32.
Tone Selection – Real or I/Q.
To generate a pattern, enter the desired parameters then click on the button labeled “Create Tones”. Click on “Send” will send the data to the TSW14xxx memory then to the DAC EVM under test. An option exist to allow the user to save this file as well.