SLWU087E november   2013  – june 2023

 

  1.   1
  2.   High Speed Data Converter Pro GUI
  3.   Trademarks
  4. Introduction
  5. Software Start up
    1. 2.1 Installation Instructions
    2. 2.2 USB Interface and Drivers
    3. 2.3 Device ini Files
  6. User Interface
    1. 3.1 Toolbar
      1. 3.1.1 File Options
        1. 3.1.1.1 User Profiles
        2. 3.1.1.2 Resize Window
      2. 3.1.2 Instrument Options
        1. 3.1.2.1 TSW14J56 and High Speed Data Converter (HSDC) Pro Eye Quality Analysis
        2. 3.1.2.2 IO Delay
        3. 3.1.2.3 JESD204B Error Injection
        4. 3.1.2.4 FPGA Registers Write Read
      3. 3.1.3 Data Capture Option
        1. 3.1.3.1 Capture Option
        2. 3.1.3.2 Trigger Option
        3. 3.1.3.3 Using Multiple TSW14xxx and ADC EVM’s for Simultaneous Capture using Trigger Option
          1. 3.1.3.3.1 Hardware Setup
          2. 3.1.3.3.2 Setting up the Slave Board
          3. 3.1.3.3.3 Setting up the Master Board
          4. 3.1.3.3.4 Read Captured Memory from the Slave Board
      4. 3.1.4 Test Options
        1. 3.1.4.1  Notch Frequency Bins
        2. 3.1.4.2  2 Channel Display and Cursor Lock
        3. 3.1.4.3  Analysis Window Markers
        4. 3.1.4.4  X-Scale in Time
        5. 3.1.4.5  Y-Scale in Voltage
        6. 3.1.4.6  Other Frequency Options
        7. 3.1.4.7  NSD Marker
        8. 3.1.4.8  Phase Plot
        9. 3.1.4.9  Phase in Degree
        10. 3.1.4.10 Histogram
        11. 3.1.4.11 Disable User Popups
        12. 3.1.4.12 HSDC Pro Lite Version
      5. 3.1.5 Help
    2. 3.2 Status Windows
    3. 3.3 Mode Selection
    4. 3.4 Device Selection
    5. 3.5 Skip Configuration
    6. 3.6 Capture Button (ADC Mode Only)
    7. 3.7 Test Selection (ADC Mode only)
      1. 3.7.1 Single Tone FFT
        1. 3.7.1.1 Parameter Controls
        2. 3.7.1.2 ADC Captured Data Display Pane
        3. 3.7.1.3 FFT Power Spectrum
        4. 3.7.1.4 Overlay Unwrap Waveform
        5. 3.7.1.5 Single Tone FFT Statistics
      2. 3.7.2 Multi Channel Display
      3. 3.7.3 Unit Selection
      4. 3.7.4 Time Domain
      5. 3.7.5 Two Tone
      6. 3.7.6 Channel Power
    8. 3.8 DAC Display Panel (DAC Mode only)
      1. 3.8.1 Send Button (DAC Mode Only)
      2. 3.8.2 Load File to Transfer into TSW14xxx Button
      3. 3.8.3 Parameter Controls
    9. 3.9 I/Q Multi-Tone Generator
  7. ADC Data Capture Software Operation
    1. 4.1 Testing a TSW1400 EVM with an ADS5281 EVM
    2. 4.2 Testing a TSW1400EVM with an ADS62P49EVM (CMOS Interface)
  8. TSW1400 Pattern Generator Operation
    1. 5.1 Testing a TSW1400 EVM with a DAC3152 EVM
    2. 5.2 Loading DAC Firmware
    3. 5.3 Configuring TSW1400 for Pattern Generation
    4. 5.4 Testing a TSW1400 EVM with a DAC5688EVM (CMOS Interface)
  9. TSW14J58 Functional Description
    1. 6.1 Testing the TSW14J58 EVM with an ADC12DJ3200 EVM
  10. TSW14J57 Functional Description
    1. 7.1 Testing the TSW14J57 EVM with an ADC34J45 EVM
  11. TSW14J56 Functional Description
    1. 8.1 Testing the TSW14J56 EVM with an ADC34J45 EVM
  12. TSW14J50 Functional Description
    1. 9.1 Device Selection
  13. 10TSW14J10 Functional Description
    1. 10.1 DAC and ADC GUI Configuration File Changes When Using a Xilinx Development Platform
    2. 10.2 DAC38J84EVM GUI Setup Example
  14.   A Signal Processing in High Speed Data Converter Pro
    1.     A.1 Introduction
    2.     A.2 FFT Calculation from Time Domain Data
      1.      A.2.1 FFT Window Correction Factor
    3.     A.3 FFT Filtering
    4.     A.4 Single Tone Parameters
      1.      A.4.1 Number of Neighboring Bins for each FFT Window
    5.     A.5 Fundamental Power
      1.      A.5.1 Harmonic Distortions
      2.      A.5.2 SNR
      3.      A.5.3 SFDR
      4.      A.5.4 THD
      5.      A.5.5 SINAD
      6.      A.5.6 ENOB
      7.      A.5.7 Next Spur
    6.     A.6 Two Tone Parameters
    7.     A.7 Average FFT Calculation
    8.     A.8 NSD Calculation
  15.   B History Notes
  16.   C Revision History
Read Captured Memory from the Slave Board

Disconnect the HSDC Pro from master board, and connect the software to slave. The user must select the device under test on the slave board again as the GUI does not keep track when using multiple boards.

Once the device is selected from the drag down menu, the message in Figure 3-15 will occur. Click OK to continue.

GUID-1FBA7229-ADC4-4285-9DD4-308F943A8CDA-low.pngFigure 3-15 Trigger Confirmation Window

In the GUI main panel, enter the sampling rate for the correct FFT processing. Once this value is entered, the captured data from the trigger event is displayed.

For the TSW14J5x, there is an advanced option available for Master/Slave triggering that is synchronized with the SYSREF signal used by the JESD204B interface. This mode enables a Master/Slave triggering synchronized with SYSREF rising edges. In master mode, a hardware output trigger is generated on the TRIG_OUT_A/B/C SMAs at the first rising edge of SYSREF that occurs after the user presses the ‘Capture’ button. The data is captured at the next rising edge of SYSREF.

In the slave triggering mode, the capture occurs at the first SYSREF rising edge following the trigger input rising edge on the TRIG_IN SMA input. This way both Master and Slave will start capturing data at the same SYSREF edge in a Synchronized manner.

Software Changes Required: (The following steps are applicable for both ADC and DAC)

To put the TSW14J5x boards in Sysref-Based Master Slave Triggering mode, add the following INI parameter just below the [Version 1.0] entry in the corresponding master and slave device INI files, as shown in Figure 3-16.

  • Sysref Based Master Slave Trigger = 1
GUID-23EE261E-DA76-4B74-9E9C-E5AF1DE2FA75-low.pngFigure 3-16 Sysref-Based Master Slave Triggering INI Setting

In the HSDC Pro GUI, select the Trigger Option menu under Data Capture Options.

For the master board, select Trigger mode enable and Arm on next capture button press.

For the slave board, select Trigger mode enable in the Trigger Option window.

HSDC Pro GUI is now configured for SYSREF-Based Master Slave Triggering. Go back to the master board and the software will do a capture on the next rising edge detected on EXT_TRG_INPUT/TRIG_IN connectors after the user clicks on the "capture" button.