DLPU072C June 2018 – January 2024 DLPC3434
This command specifies the amount of time that must pass before edges of the INT_SUBFRAME signal, which are artificially inserted ensuring the edges never stop completely. The input parameters are applied separately to the axes defined by AWG_12 and AWG_34.