SLVSJQ6 September 2025 TMF0064
PRODUCTION DATA
Table 6-1 is a memory map of the 64768-bit FRAM section of the TMF0064 device, configured as 253 pages with 32-bytes each. Eight adjacent pages form one 256-byte block. The 32-byte volatile scratchpad buffer is used when programming the FRAM memory. The process for writing to the FRAM memory includes two steps. Data is first written to the scratchpad buffer. The data is then verified by reading the scratchpad buffer that confirms proper receipt of the data. If the buffer content is correct, a copy scratchpad command is issued to copy the scratchpad buffer to the FRAM memory. This process verifies data integrity when programming the memory. See Section 6.5.4 for details regarding programming and reading the 7680-bit FRAM portion of the TMF0064.
| ADDRESS RANGE | TYPE (1) | DESCRIPTION | PROTECTION CODES (NOTES) |
|---|---|---|---|
| 0000h to 00FFh | R/(W) | Data Memory Pages 0 to 7 (Block 0) | (Protection controlled by address 1FA0h) |
| 0100h to 01FFh | R/(W) | Data Memory Pages 8 to 15 (Block 1) | (Protection controlled by address 1FA1h) |
| 0200h to 02FFh | R/(W) | Data Memory Pages 16 to 23 (Block 2) | (Protection controlled by address 1FA2h) |
| 0300h to 03FFh | R/(W) | Data Memory Pages 24 to 31 (Block 3) | (Protection controlled by address 1FA3h) |
| 0400h to 04FFh | R/(W) | Data Memory Pages 32 to 39 (Block 4) | (Protection controlled by address 1FA4h) |
| 0500h to 05FFh | R/(W) | Data Memory Pages 40 to 47 (Block 5) | (Protection controlled by address 1FA5h) |
| 0600h to 06FFh | R/(W) | Data Memory Pages 48 to 55 (Block 6) | (Protection controlled by address 1FA6h) |
| 0700h to 07FFh | R/(W) | Data Memory Pages 56 to 63 (Block 7) | (Protection controlled by address 1FA7h) |
| ... | ... | ... | ... |
| 1D00h to 1DFFh | R/(W) | Data Memory Pages 232 to 239 (Block 29) | (Protection controlled by address 1FBDh) |
| 1E00h to 1EFFh | R/(W) | Data Memory Pages 240 to 247 (Block 30) | (Protection controlled by address 1FBEh) |
| 1F00h to 1F9Fh | R/(W) | Data Memory Pages 248 to 252 (Block 31) | (Protection controlled by address 1FBFh) |