SCPS287D November 2023 – September 2025 TPLD1201
PRODUCTION DATA
Combinational logic is supported through lookup tables (LUTs) within the TPLD1201 including two 2-bit LUTs and two 3-bit LUTs. Inputs and outputs for the combination function macro-cells are configured from the connection mux with specific logic functions being defined by the state of OTP bits.
The TPLD1201 has seven combinational function blocks (macro-cells) that can serve more than one logic or timing function. In each case, they can serve as a lookup table (LUT), or as another logic or timing function. See the following list for the functions that can be implemented in these logic blocks: