SLVSDO6D August 2017 – December 2024 TPS1H000-Q1
PRODUCTION DATA
A high-accuracy current limit allows high reliability of the design. It protects the load and the power supply from overstressing during short-circuit-to-GND or power-up conditions. The current limit can also save system cost by reducing the size of PCB traces and connectors, and the capacity of the preceding power stage.
When a current-limit threshold is reached, a closed loop activates immediately. The output current is clamped at the set value, and a fault is reported out. The device heats up due to the high power dissipation on the power FET.
The device has two current-limit thresholds.

Note that if using a GND network which causes a level shift between the device GND and board GND, the CL pin must be connected to the device GND.
For better protection from a hard short-to-GND condition (when the IN pin is enabled, a short to GND occurs suddenly), the device implements a fast-trip protection to turn off the output before the current-limit closed loop is set up. The fast-trip response time is less than 1 µs, typically. With this fast response, the device can achieve better inrush current-suppression performance.
Figure 6-1 Current Limit